Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
LM20K Family PowerWise Synchronous Buck Regulator Slide 19

This circuit uses the PGOOD pin to control the enable pin of Device2. When the voltage at VOUT1 reaches approximately 95% of its final value, the PGOOD pull down FET will turn off and the voltage will rise to EXTVCC (2.7V) to enable Device2. The PGOOD pin can also be used to sequence loads that have a RESET or ENABLE input.

PTM פורסם ב: