Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
LM20K Family PowerWise Synchronous Buck Regulator Slide 27

Operating the devices in parallel and out of phase allows for twice the output current while maintaining the same net efficiency. The power dissipation is also distributed between the two devices resulting in a cooler running solution. Like the previous example, the RMS input current is greatly reduced. In fact, for duty cycles near 50%, the RMS input current can approach zero.

PTM פורסם ב: