Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
LM20K Family PowerWise Synchronous Buck Regulator Slide 20

This circuit shows how the LM3880 can be used to sequence multiple devices. The LM3880 allows for multiple sequences and is factory configurable. Note that pull-up resistors on the flag outputs are not needed on the LM20242 high voltage device since the enable pins have an integrated pull-up current source. Pull up resistors would be needed on all of the low voltage LM20xxx devices.

PTM פורסם ב: