Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
LED Driver Overview Slide 22

If dimming is required of a lighting system, one must consider this when selecting an LED driver. There are two predominantly used methods for dimming in North America. The first is line voltage dimming via phase-cutting with a TRIAC. This method is quite straight forward and is commonly used for dimming incandescent lamps. It is, however, much less commonly used for LED dimming as it requires a fair bit of extra engineering to design an LED driver that works effectively with these phase-cut waveforms. The second method is a 0-10 V 2-wire signal interface. This dimming protocol is commonly used for commercial fluorescent dimming in North America. Furthermore, as a result of its common usage, controls utilizing this protocol are widely available.

PTM פורסם ב: