Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
LED Driver Overview Slide 4

There are two major types of LED drivers, Constant-Current and Constant-Voltage. Most drivers are constant-current. This type is preferred by LED manufacturers as it provides better control over LED operation. Constant-voltage drivers are typically only used when the LED current is regulated on the light engine itself.

PTM פורסם ב: