Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
LED Driver Overview Slide 23

There are two methods used for dimming LEDs. The first is by simply reducing the DC current flowing through the LED. This is the simplest and most straight forward method of dimming. An alternative method is pulse width modulation, or PWM. This method maintains the same peak current flowing through the LED and accomplishes dimming by switching the LED on and off at a fixed frequency with varying pulse widths, thereby reducing the average current and apparent brightness of the LED.

PTM פורסם ב: