Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
LED Driver Overview Slide 6

At a fixed voltage, the current flowing through the LEDs can vary dramatically depending on the forward voltage of the individual LED array. For instance, the example here shows that the minimum, typical, and maximum currents for a 400 lumen cool white LED Array with an applied voltage of 8.4 V could be 0 mA, 70 mA or 300 mA, respectively, depending on the forward voltage of the array. If this voltage was applied to adjacent LED Arrays, one would appear to be out (0 mA), one dim (70 mA) and one bright (300 mA).  It is for this reason that the LED manufacturers recommend against driving LED arrays with constant voltage sources or connecting multiple LED arrays in parallel.

PTM פורסם ב: