Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
THM-Slide1

Welcome to the TRACO Power THM Series product training module. This presentation will bring awareness to medical DC/DC converters that manufactured by TRACO Power, specifically the THM family of products. It will explain how to meet Medical Applied Parts requirements and show how a DC/DC converter approach can help achieve the 2xMOPP requirements for Applied Parts. An overview of the THM family of medical DC/DC converters, covering 3 Watts to 30 Watts and their safety and compliance characteristics will be explained, followed by common key features that the THM series shares across all power levels, as well as features that help solve medical system requirements that are needed to meet a 2xMOPP rating. The next section will introduce our featured product, the THM-30WI series, and highlight how this increased output power of a 30W DC/DC converter, in a 2” x 1” package with wide inputs can help solve higher power requirements. Following this, we will explain the THM-30WI Series’ compliance and safety agency certifications, as these are critical for medical grade applications. The next slide will show examples of typical applications that the THM Series commonly fits into. Lastly, it will provide a summary of the evolving medical market and how TRACO Power medical DC/DC converters can help support the next generation of medical equipment products, including the latest compliance for B or BF rated equipment.

PTM פורסם ב: