Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
SmartOnline Single-Phase UPS Systems Slide 11

One way a UPS system can help ensure continuous availability is to include redundant (or "extra") components within its chassis, known as "N+1" redundancy. Tripp Lite "N+1" Single-Phase UPS systems (available in 12, 16 and 20 capacities) feature two UPS power modules for internal "N+1" redundancy. If one power module is removed for maintenance, the other power module will support the equipment load (as long as it does not exceed the capacity of the power module). Like other modules, Tripp Lite N+1 Single-Phase UPS systems also include a hot-swappable power distribution module to ensure continuous availability if both power modules need to be removed for maintenance.

PTM פורסם ב: