Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
SmartOnline Single-Phase UPS Systems Slide 17

Switching between Tripp Lite SmartOnline Single-Phase UPS systems' two high-efficiency modes (Economy and On-Line) is easy. Managers can configure one UPS or mass-configure multiple UPS systems remotely through PowerAlert software. All that is required is PowerAlert Local Software (included free of charge with all Network UPS systems) and an internal SNMP/Web card (available separately from Tripp Lite) installed in the UPS. Using PowerAlert, managers can set the mode once, or can schedule a reoccurring change back and forth between modes as the application dictates. For example, a manager may want to schedule UPS systems to run in On-Line mode during the day on weekdays, but automatically switch to Economy mode in the evenings and on weekends.

PTM פורסם ב: