Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Effortless Scalability

Continuing to look at the physical size and visual comparison, even with a bigger housing the GM3 heatsink mounting hole pitch is the same as the smaller FM3 package at 53 mm. This means that upgrading from the FM3 to the GM3 does not require significantly more footprint area. If the consideration is made beforehand, the module pitch can be set to enable the use of the same heatsink for both FM3 and GM3-based systems. So with the physical transition relatively simple, the system can be scaled or upgraded with the GM3 in terms of electrical performance.

PTM פורסם ב: