Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
GM3 Further Bridges the Gap

To better understand how the GM3 fits into the power continuum, here is a visual aid demonstrating a 1:1 scale size comparison to the smaller FM3 WolfPACK™ package and the larger SiC-optimized XM3 footprint. With 11 and 16 mΩ half-bridge versions in the FM3 package, the slightly larger GM3 package reduces the on-resistance offerings to 6 and 8 mΩ. This theme continues with the larger, yet relatively small XM3 half-bridge module variants, offering low on-resistance down to 2.6 mΩ. So again, the GM3 further bridges the gap between the FM3 and the higher power module solutions in terms of on-resistance, power, and size.

PTM פורסם ב: