Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Power Elements Press Fit Slide 9

The bush and shank terminals with-full pin plating have no hole through the Power Element, which means the cable needs to be mounted to the top of the element by a screw (adjusted to the size of the hole) or by a nut on the shank. These elements are available from nine, up to thirty six, pins with bush/shank configuration from M3 to M10.

PTM פורסם ב: