Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
IO-Connector-Slide12

The Delta or D Ribbon connector combines the virtues of the ribbon-style contact with many of the positive attributes of the D Sub connector. It is commonly used for low speed parallel port connections meeting IEEE 1284-B, such as  legacy storage devices, or communications equipment between shelves or cabinets. The 3M™ 3000 Series is offered in popular sizes with metal shells for protection from EMI/RFI when mounted at the I/O slot.

PTM פורסם ב: