Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
NEMA-Slide18

The issues to consider may be very basic. For example, if maintenance may need to be done on a product, or frequent access to the internal components is required, the type of latching device can be meaningful. Using a knob or key lock would be helpful in this situation but when access is less frequent, a more secure screw closure would be sufficient. Also, making sure that equipment/wall mounting brackets can be used with the enclosure saves time and money.

PTM פורסם ב: