Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
NEMA-Slide21

Some materials are easier to drill than others, or may require special tools and bits. If the installer improperly drills a hole into a plastic box, they run the risk of it cracking. Brackets are also harder to install after the fact on a plastic box than on a steel. If a special finish is required, it must be molded into both plastic or fiberglass, whereas it can be added later on the metal enclosures.

PTM פורסם ב: