Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
NEMA-Slide4

Bud recently ran a survey and uncovered that over 70% of engineers were often confused by the many different NEMA ratings. This led to another survey that suggested that up to 40% of all enclosures that require protection are specified to the wrong level. For some, it is using an enclosure that does not provide the complete protection desired. For others, they specify the most popular level, which is not required, spending more for unnecessary protection levels.

PTM פורסם ב: