Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
NEMA-Slide20

The final common error is specifying an enclosure without thinking about how it may need to be modified. Most NEMA enclosures need to have some sort of modification to allow for input and output. Some enclosure types are easier to modify than others. For example, if the end use requires a special color, steel or die cast aluminum would be the logical choices. 

PTM פורסם ב: