Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
NEMA-Slide8

The numbering system of NEMA is inconsistent with NEMA 4 being more protective than NEMA 12, leading to a major misconception by engineers and purchasing staff. NEMA 4 enclosures can be used both indoors and outdoors. It protects against everything that NEMA 12 protects against plus falling and sprayed liquids and the formation of ice. This is the product to use in a factory where there may be spray cleaning or where the box is used outdoors. There is typically an increased cost when compared to NEMA 12, so it is important that the engineer specify the proper level.

PTM פורסם ב: