Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Slide11

The EPCOS brand of input and output filter capacitors is available as boxed film capacitors in the series and types for the MKP DC Link versions. They feature a wide range of capacitance values as well as a wide range of voltages, a maximum operation temperature rating of 105°C, and current rating up to 108 A.

PTM פורסם ב: