Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Slide23

In addition to hybrid and electric automobiles there are various similar charging and discharging applications where an on-board charger is present. These are application such as material handling equipment, mass transit vehicles, golf carts, and airport ground support equipment. The PTC-ICL components fit the same applications. The J-series types offer an added benefit; they are ideally suited for harsh environments due to the encasement in which the PTC-ICL disc is housed. This aids in the prevention of dirt, dust, and similar contamination ingress.

PTM פורסם ב: