Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Slide19

The EPCOS brand PTC-ICLs are available in a variety of both leaded through-hole types and the encased types. The number of devices required can be calculated using the formulas shown on this slide, based upon the electrical energy equal to the thermal energy. The devices can be connected in parallel as required.

PTM פורסם ב: