Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Slide24

As illustrated in the block diagram on this slide, in a hybrid bus application there is also a DC-Link function and battery bank which requires the same PTC-ICL component for safely discharging the battery system. In this application for higher voltages the PTC-ICL device can be used in a parallel circuit configuration.

PTM פורסם ב: