Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Slide12

The EPCOS brand of input and output filter capacitors is available as boxed film capacitors in the series and types for the MKP DC Link versions with a wide range of capacitance values as well as a wide range of voltages with a max operation temperature rating of 105 Degrees Celsius and current rating up to 108 Amps.

PTM פורסם ב: