Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
AOA with vinculum ii
Another FTDI solution that also uses the Android Open Accessory mode is FTDI’s Vinculum-II (VNC2) family of ICs and modules. This is a single-chip embedded host which can be programmed to include the AOA support. In addition to the interfaces available with the FT311D IC, the Vinculum-II also includes a second USB port that can be configured as a USB host or USB device. With the second USB port of the Vinculum-II configured for host, it is possible to add USB support for traditional USB peripherals such as a barcode scanner that already uses an FTDI peripheral IC or connects as a HID peripheral.
PTM פורסם ב: