Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
developing apps with d2xx
To develop applications using the FTDI Java D2XX for Android driver, the development machine needs the Eclipse IDE and an up-to-date Android SDK, including the ADB program and the ADT plug-in for Eclipse. Installation and configuration of these tools is outlined on the Android development web site. Please see (http://developer.android.com/sdk/index.html). The Android device should also have USB Debugging enabled to allow access using the ADB utility. To accomplish this for the Android platform, navigate to Settings > Applications > Development and select the USB debugging option.
PTM פורסם ב: