Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
usb host or usb device
The first interface factor to consider is whether the Android platform supports USB host. Android smartphones always provide a USB device port but some Android tablets provide both USB host and USB device ports. The USB device port is for connecting to a PC or embedded host to enable data transfer and battery charging. The USB host port is for connecting to USB peripheral hardware. Many Android platforms are now supplied with On-The-Go (OTG) USB ports, which allow for the USB port to be either a host or a device. Some of these OTG ports will be USB device only and some will offer both USB host and device capabilities. One way to determine if a user’s Android platform supports USB host and/or device is by the cable type. A Micro-AB cable will likely be both USB host and device, whereas a Micro-B cable will indicate USB device only.
PTM פורסם ב: