Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
rtrim and nomical vout
The next step is to tell the GUI what value (in KΩ) of trim resistor is being used on the evaluation board. The factory default setting is 1.2 V output, so the corresponding trim resistor is 20 KΩ. Once that has been entered as the Rtrim value, the Nominal Vout box will display the set point of 1.2 V.
PTM פורסם ב: