Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
oc fault red
Notice that the Over current warning is still on. This is actually by design. All faults must be cleared by clicking the “Clear Faults” button. This allows the master controller to retain any fault events until they are actively cleared. This happens even if the faults have passed. For example, if a short duration pulse of 6 A were to occur with an average current of 2 A, then setting the OC warning below 6 A would capture the event. This is because a fast transient is tripping the fault, and the module retains this fault until the user chooses to clear it. This allows the user to capture faults that occur faster than the PMBus time resolution would allow.
PTM פורסם ב: