Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
KeyPad-Slide10

Volume Resistivity is the strength of Gap Pad reducing the flow in electric leakage current. A low number (in Ω•m or Ω•cm) refers to superconductor while a high number 1016 refers to an insulator. ASTM D257 is the standard used in testing this parameter. A standard size specimen is placed between two electrodes for sixty seconds, a voltage is applied and the resistance is measured. Surface or volume resistivity is calculated, and apparent value is given (60 seconds electrification time).

PTM פורסם ב: