Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
KeyPad-Slide14

Compression deflection refers to resultant forces a material exerts while being deflected. As a compressive load is applied, the elastomer material is deformed but the volume of the material remains constant. The compression deflection characteristics can vary, depending on the material geometry (example of thickness, size and surface area), rate of deflection, size of probe, and other parameters.

PTM פורסם ב: