Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
KeyPad-Slide8

Shown here is the table of electrical properties definitions. ASTM standards and procedures are used to determine these electrical thermal properties. Different TIMs vendors might use different methods/standards of testing. It is always highly recommended for the designer to test in the actual application to remove variables that are not taken into account with different standards. Moreover, humidity and elevated temperature can significantly lower the results in the electrical properties significantly.

PTM פורסם ב: