Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
KeyPad-Slide6

Thermal Impedance is a measure of the total resistance to the heat flow from a hot surface to a cold surface via thermal interface materials. Area and interfacial resistance are taken into account comparing to thermal resistance (which does not). Thermal impedance is measured using ASTM D5470.

PTM פורסם ב: