Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
KeyPad-Slide7

To account for the thermal performance, it is important to consider that all of the thermal resistances are taken into account. The example shown here shows the different level of interfacial resistance that needs to be taken into consideration to determine the thermal performance. Clamping forces at 10% compression on Gap Pad material with TO-220 (heat source) allows the designer to determine the pressure vs thermal impedance.

PTM פורסם ב: