Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
DigitalPower-Slide19

From the PowerNavigator launch screen, there are two ways to access the digital power monitors (DPM). In the offline mode, the DPM can be selected from the PowerNavigator Library. If the evaluation kit is available or the user’s hardware with DPM, it can be connected to the PC and the PowerNavigator GUI will automatically pick up what devices are available and the corresponding address. In the example shown, two ISL28023 evaluation boards were connected. A total of up to 55 DPM can be connected, if so desired.

PTM פורסם ב: