Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Product List
MAX2870-Slide28

A key design aspect of the MAX2870 is the bank of fundamental VCO’s with sub-bands that enables ultra-wideband operation. There are four individual VCO core blocks with a fundamental frequency range of 3000MHz to 6000MHz. Each VCO block has 16 sub bands. A state machine based VCO auto-select function is used to automatically select the correct VCO. Manual VCO selection is also possible with the appropriate register setting.

PTM פורסם ב: