Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Product List
MAX2870-Slide8

This example illustrates how the PLL synthesizer is used as the LO in a typical radio receiver. The LO working with the down mixer is used to frequency translate an RF carrier down to a lower intermediate frequency. In this case the RFIN spectrum ranges from 5725MHz to 5825MHz. The RF spectrum example is the upper range of the Unlicensed National Information Infrastructure ISM band. For this example, the radio receiver will sequentially tune to one of four 20MHz channels occupying the RF input spectrum.

PTM פורסם ב: