Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Image of MoSys Accelerator Bandwidth Engine: High Performance/High Bandwidth - Out of the Box

As a result of the unique architecture of the Peraso accelerator engines, it not only supports the standard read/write accesses of a standard RAM device but because it also has two ports that can operate in tandem or separately, it is possible to use the BE3 device as a dual ported structure allowing independent access from each of the two ports. These devices are ideal to be used as statistics engines, oversubscription buffers, fast lookup tables, and even graphics convolution buffers. Due to the high-speed, high random access rate, unique architecture, and increased density, it opens up the option of a next generation RAM for newer high-speed systems.

PTM פורסם ב: