Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Image of MoSys Accelerator Bandwidth Engine: High Performance/High Bandwidth - Quazar and Blazar Families

This is an illustration of the Peraso families of accelerator engine ICs. Each family includes 576Mb devices (which is four times the density of the most popular QDR device) as well as 1Gb devices (which is eight times the density of QDR). The Peraso devices are single die monolithic ICs and support SerDes interface rates up to 25Gbps.

PTM פורסם ב: