Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Image of MoSys Accelerator Bandwidth Engine: High Performance/High Bandwidth - Product Lines

Peraso offers three lines of semiconductor ICs and a line of IP to support packet classification. The three IC families are Quazar low-cost, high-speed devices to address the QDR and synchronous SRAM market, Blazar to address the high-speed increased (in-memory) functionality, to provide a path to even higher system performance. The Blazar family also includes the Programmable HyperSpeed Engine (PHE) Device that is comprised of 1Gb of memory and 32 multi-threaded RISC cores all on a single die, and LineSpeed is a group of SerDes based Phy products to support 100G Gearbox, Retimer and 2:1 Mux functionality. There is a fourth family, however it is not an IC product, but an IP offering. Stellar is the newest family and it is a series of packet classification IP offerings that is available as RTL, which runs on either Intel or Xilinx FPGAs.

PTM פורסם ב: