Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Image of MoSys Accelerator Bandwidth Engine: High Performance/High Bandwidth - Memory Architecture is Critical

Shown here is a single (monolithic) device from Peraso that can support greater throughput while providing the density of four QDR devices or eight QDR devices with the 576Mb or 1Gb devices that are available in production from Peraso. In addition to the significant board space savings and the reduced number of devices offered, it also reduces power (and possibly the associated power supplies and regulators). It also requires a fraction of the PCB board traces which can save PCB layers and layout time. Each of the areas of physical space, power, reliability, supporting RTL, pure access speed, and latency are addressed by the Peraso accelerator engine families.

PTM פורסם ב: