Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Bridge Solutions Slide 10
These devices can be used in application where a UART is needed, and because of the nature of the serial bus interface the number of connections between the host and the UART are greatly reduced. This allows smaller packages to be created, and that make them ideal for cell phone, battery-powered devices. They can also be used in the typical UART applications: point of sale, Bluetooth/GPS interface, and IrDA applications.
PTM פורסם ב: