Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Bridge Solutions Slide 22
I2C is becoming a popular method for controlling multiple devices within the same board or across boards. There are many devices that use I2C as a main interface to the host, and this bridge can be easily used to control these devices. SPI is a matured and well understood bus; many, if not most of microprocessors and embedded processors support this interface. These devices allow the processor to add support for I2C.
PTM פורסם ב: