Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Bridge Solutions Slide 23
This slide shows a typical application for this Bridge. There are three I2C devices connect to the Bridge’s I2C bus: an EEPROM, a LED dimmer and a GPIO expander. The SPI-based host sends and receives data from any of these three devices by sending the physical address of the particular device along with the data (commands) to the Bridge. The Bridge will then translate these data (commands) to I2C electrical signals on the I2C bus. It then sends the host’s data (commands) to the correct device. This device supports multi-master I²C networks.
PTM פורסם ב: