Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Bridge Solutions Slide 16
Because of the hardware simplicity of the UART interface and the ease of writing software, this bridge device offers many advantages over other solutions: two wire host interface, long distance communication through RS-232, and no interrupt pin is need to interrupt the host – data is sent to the host automatically. The UART on the host side will interrupt the host if enabled. In addition, there are only a few commands that need to be learned and these commands can do everything a typical I2C controller is supposed to do, small 16 pin TSSOP package, eight extra GPIO pins available for use.
PTM פורסם ב: