Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
RF Small Signal Products Part 2 Slide 10
For a series SPST (Single Pole, Single Throw) switch has a minimum Insertion Loss over a wide range of frequency. Insertion Loss depends on the forward resistance of the diode and Isolation depends on the capacitance of the diode. The operations are very straight forward. When forward biased, the SPST switch is “ON” and When reverse biased, the SPST switch is “OFF”.
PTM פורסם ב: