Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
RF Small Signal Products Part 2 Slide 8
In RF frequencies, the PIN Diode can be seen as a circuit diagram as shown on the right hand side. The topology may differ slightly under different biasing conditions. When the diode is forward biased, the upper right equivalent circuit can be used. In here, the variable resistance, which is as a function of forward current flowing through the diode, expressed in formula form. Rs is the contact and metal resistance and the Cp is the package capacitance. The parameters k and x are empirical constants. When zero or reverse biased, the lower right equivalent circuit is valid. Here the package has an important contribution to the high frequency behavior of the device.
PTM פורסם ב: