Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
RF Small Signal Products Part 2 Slide 22
First, for each Varactor diode on the wafer four to five samples are taken for Capacitance at different voltages. Then, for each (x,y) coordinates are recorded and parameters such as Vbr (breakdown voltage) and IR (reverse diode current) are checked. Finally, all diodes are matched by a PC to be used in an assembly sequence file. The diagram below illustrates the steps in which it shows the DMA sequencing, Diode assembly and testing, and finally taping the DMA matched Varactor diodes.
PTM פורסם ב: