Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
RF Small Signal Products Part 2 Slide 28
VCO, also called Voltage Controlled Oscillaor, is a combination of components (like resistors, capacitors and transistors) to oscillator and store RF energy in order to create a certain frequency by changing the voltage. VCXO, also called Voltage Controlled X-tal (crystal) Oscillator, is a x-tal oscillator controlled by a voltage. A x-tal is cheap and temperature sensitive element which must be controlled by a voltage for frequency stability within a few percent in variation, that is sufficient for applications such as cellular phones. TCXO, also called Temperature Controlled X-tal (crystal) Oscillator, is a temperature controlled X-tal oscillator with a reduced temperature  dependence of the resonance frequency. By using a temperature sensor controlling the tuning voltage stability in the ppm range is attained.
PTM פורסם ב: