Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
RF Small Signal Products Part 2 Slide 14
Here we illustrate how to construct a Series-Shunt SPDT switch. Only in the transmit state we have to apply biasing, and both diodes are forward biased. D1 is a low impedance TX to Antenna. D2 is a high impedance at the antenna due to the ¼ length section. In the receive state both diodes are reversed biased, open, no current consumption during receive mode! One drawback, just as in previous example, is that it’s frequency dependent due to ¼ length section.
PTM פורסם ב: